5/19/2020 1:18 PM | |
Joined: 10/10/2017 Last visit: 7/21/2024 Posts: 61 Rating: (0) |
Yes, in this case, I have done the hardware configuration, and commissioning and programming using Simotion Scout. |
5/20/2020 8:25 PM | |
Joined: 10/10/2017 Last visit: 7/21/2024 Posts: 61 Rating: (0) |
Hi, I have done all the listed steps from configuring PROFINET addresses and I have downloaded script for generating GSDML from this site https://support.industry.siemens.com/cs/document/92022677/sinamics-g-s%3A-generating-gsdml-files-for-s120-s150-g130-g150-s110?dti=0&lc=en-DE Is there anything I can do to generate GSDML file? |
5/22/2020 8:13 AM | |
Joined: 5/12/2006 Last visit: 9/18/2024 Posts: 22364 Rating: (3011)
|
in step7 hw config options you can generate the gsd file |
Follow us on