5/21/2020 7:26 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating: (1) |
qwazee thank you for advice regarding to hmi. Now my problem is that I can't connect with plc. I am using cable like on photo - profibus to usb - but I can't communicate with plc. I have setup pg/pc interface to usb connection - like on photo. Do you think it is problem of a cable/adapter that I am using ? my plc is cpu-314 6ES7 314-1AG13-0AB0 KR Leszek |
Last edited by: Leszek Jaszczak at: 05/21/2020 19:27:57 |
|
5/21/2020 7:33 PM | |
Joined: 3/30/2020 Last visit: 9/25/2024 Posts: 4789 Rating: (982) |
The USB setting you are trying to use is not what you think it is. The cable you are using looks like a USB to RS232 converter cable. It will not work. That is an MPI port on the PLC. You need an MPI cable. Other volunteers may come in and tell you exactly which part number you require. The PLC will not program without it, unless you get some other expensive gear. But you had a teleservice card. Which one is it. This could be the 'expensive gear' you need. Do a search in the search bar in this site to supply some documents about the teleservice card. Good luck. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
5/21/2020 8:03 PM | |
Joined: 2/5/2013 Last visit: 9/24/2024 Posts: 321 Rating: (74) |
Hi, Please click on below link: You need below MPI Cable mentioned in attached pdf.
Br, AmolG Attachment6GK15710BA000AA0_datasheet_en.pdf (116 Downloads) |
Please rate it. |
|
5/21/2020 8:13 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating: (1) |
qwazee I have TSA MODEM with usb Do you think I can connect cpu 314 via prfibus to tsa modem and then modem to plc using usb ?
|
5/21/2020 8:32 PM | |
Joined: 3/9/2018 Last visit: 8/31/2024 Posts: 189 Rating: (14) |
According Google it seems you can with a USB cable or with a RS232 nul-modem cable. See page 35/36 5.2 Installing the software Procedure 1. Insert the supplied "SIMATIC TeleService Edition" CD into the CD-ROM drive of your PC. 2. The setup program starts automatically and guides you through the installation. If the autostart function for your CD-ROM drive is disabled, run the setup program by doubleclicking Setup.exe in the root folder of your "SIMATIC TeleService Edition" CD. 5.3 Setting the PG/PC Interface Procedure During installation of the software you are prompted to set the PG/PC interface. 1. In the "Set PG/PC Interface" dialog, check whether the following interface parameter has been assigned. The selection list must contain the entry: – TS Adapter If this is not the case, – click "Select..." to add/remove an interface. The "Install/Remove Interface" dialog box opens. – Select the "TS Adapter II" module from the selection list and install the adapter. Click "Close" to close the dialog box. 2. In the "Set PG/PC Interface" dialog, select the interface parameter assignment that you want to use in the future for communication (TS Adapter). Click the "Properties" button. 3. The "Properties - TS Adapter" dialog box opens. Open the "Local Connection" tab. Set "USB" as the direct connection. 4. Click "OK" to close the "Properties - TS Adapter" dialog box. 5. Click "OK" to close the "Set PG/PC Interface" dialog box. 6. If you have changed an access path in these settings, a warning message then appears. To apply the changes, click "OK". Attachmentts_adapter_II_manual_en-US.pdf (94 Downloads) |
Last edited by: Henry1675 at: 05/21/2020 20:34:32Last edited by: Henry1675 at: 05/21/2020 20:39:28Last edited by: Henry1675 at: 05/21/2020 20:40:32 |
|
This contribution was helpful to1 thankful Users |
5/21/2020 8:52 PM | |
Joined: 4/3/2019 Last visit: 2/20/2024 Posts: 116 Rating: (1) |
Henry1675 thank you I have tryied but first I don't have cd and secon there is no option for usb in settings lie on photo I will try to download - TeleService V6.1 incl. SP5 and install it maybe this will help |
Last edited by: Leszek Jaszczak at: 05/21/2020 20:54:01 |
|
Follow us on