12/16/2008 12:24 PM | |
Joined: 4/12/2007 Last visit: 9/3/2020 Posts: 9 Rating: (0) |
Hi there, What I need to do is change the on delay times of all the timers when I change one. Please see attached. I need the time delay of timers 2 and 3 to change automatically when I change timer 1 Attachmenttimers.pdf (483 Downloads) |
12/18/2008 12:38 PM | |
Posts: 661 Rating: (123) |
Hi course you can. Please look at the example "Using the reference function": http://www.automation.siemens.com/logo/html_76/products/02Applications/index.html (example on page 4). You need a LOGO! 0BA5 or 0BA6. The setpoint for the timers (on-time)you enter in V1 of the analog MUX. Then you refer the on time of alll timers to the MUX. V1 of the MUX you can display in a messagfe text. So it´s very easy to adjust thevalue quickly. AttachmentSetpoint via MUX.zip (478 Downloads) |
Follow us on