5/23/2020 5:28 PM | |
Joined: 2/5/2013 Last visit: 4/25/2024 Posts: 320 Rating: (74) |
Hi Eufrásio332020, Please post your next post in English. Not everyone in this forum understand Portuguese.
|
Please rate it. |
|
This contribution was helpful to1 thankful Users |
5/23/2020 5:37 PM | ||||
Joined: 2/5/2013 Last visit: 4/25/2024 Posts: 320 Rating: (74) |
Hi , For CPU 313C 6ES7313-5BG04-0AB0 V3.3 CPU 313C available below programming package.
Br, AmolG. Attachment6ES73135BG040AB0_datasheet_en.pdf (198 Downloads) |
|||
Please rate it. |
||||
5/23/2020 6:41 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665)
|
Hello Eufrásio; As shown by AmolG, you need at minimum Step 7 v5.5 SP1. Siemens offers a trial download of Step 7 v5.6, you can find the link here: https://support.industry.siemens.com/cs/us/en/view/109761679 A trial license makes the software completely functional, without restrictions, for a period of 21 days. Once it is expired, you must install a valid license to continue. Since the trial license is time-limited, you should take a few moments to consider how you will connect the programming PC to the CPU, before you install the trial version. Do you have a programming cable or interface at this time? A USB/PC Adapter (MPI interface CP 5711) is the least expensive option, if you need a new cable. See the screenshot below. Daniel Chartier Edit: Could you explain this a bit more: "gostaria de copiar ou programar segurança, para nenhum caso dela não funcione mais.", I am not sure you mean you want to correct a malfunctionning CPU or if you would need to program a Safety application, such as E-Stop, sith SIL 2 or SIL 3... D.C. |
Last edited by: dchartier at: 05/24/2020 01:19:37 |
|
This contribution was helpful to1 thankful Users |
5/25/2020 5:44 PM | |
Posts: 2 Rating: (0) |
Muito obrigado pelo seu apoio! |
Follow us on