5/12/2020 7:57 AM | |
Joined: 12/18/2014 Last visit: 9/26/2024 Posts: 33838 Rating: (4205) |
Are both plc in the same subnet? |
5/12/2020 8:15 AM | |
Joined: 4/23/2011 Last visit: 9/17/2024 Posts: 39 Rating: (0) |
yes of course! Sometimes suddenly connected for some seconds and the this fault appears again |
5/12/2020 11:35 AM | |
Joined: 4/23/2011 Last visit: 9/17/2024 Posts: 39 Rating: (0) |
No |
5/12/2020 1:18 PM | |
Joined: 4/23/2011 Last visit: 9/17/2024 Posts: 39 Rating: (0) |
I send you screenshots from the logo program which is simple and the settings from the s7-1200 if you want anything else tell me Thank you in advance AttachmentScreenshot 2020-05-12 12.59.22.zip (89 Downloads) |
5/12/2020 8:35 PM | |
Joined: 4/23/2011 Last visit: 9/17/2024 Posts: 39 Rating: (0) |
I send you the logo program. The s7-1200 program is too big to send it from here tell me how to send it AttachmentCircuit Diagram.zip (111 Downloads) |
Follow us on