5/27/2020 10:56 PM | |
Joined: 11/28/2019 Last visit: 3/24/2024 Posts: 20 Rating: (0) |
Hello, What is the procedure to do this Update from TIA V14 To V15 ??? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/28/2020 09:20:30New subject after splitting |
|
5/28/2020 12:29 PM | |
Joined: 8/31/2005 Last visit: 4/26/2024 Posts: 2197 Rating: (326) |
Just install the V15. I'm not sure the setup will upgrade the V14 licence to V15 (with the update license) . If not, you can use the Automation license Manager to update the V14 license with the update license to a V15 license. After the licence update in ALM, you only have a V15 license on your PC. The TIA Portal V14 will work with the V15 license too. So you can use both versions. When you open a V14 project in V15, the project will be updated to V15. By default it is saved under an other name ( _V15 is added) Instead of installing the V15, you should install the V15.1. (Runs with V15 license). |
Last edited by: miami at: 05/28/2020 17:22:17corrected link to trail version download |
|
This contribution was helpful to1 thankful Users |
5/28/2020 5:32 PM | |
Joined: 11/28/2019 Last visit: 3/24/2024 Posts: 20 Rating: (0) |
Thank you Miami for your assistance ^_^ |
5/28/2020 6:05 PM | |
Joined: 3/30/2020 Last visit: 4/26/2024 Posts: 4455 Rating: (931) |
Hello. please allow me to attempt to cover more angles. You can have several versions of the software installed on your PC. TIA Portal V14, V15 and V15.1 can be installed and work from the V15 license. Did you buy an upgrade? Which license do you need to upgrade from Look for sentence: "Proceed as follows to upgrade a License Key". Do not mind the fact that V16 is mentioned - the concept stays in place. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on