5/29/2020 11:54 PM | |
Joined: 12/29/2019 Last visit: 2/23/2024 Posts: 3 Rating: (0) |
Hello, I have this exact same issue, exact same issue except I always Compile -----> Software (rebuild all) before saving and downloading Software (download all). I am using the following:
My I/O Field is set for the following:
I can enter the value into the I/O field and it accepts the value, but will not write the value to the DB. It keeps the same value when changing pages and coming back to the page. I have checked the HMI tag link to the PLC tag link and deleted/added back I/O field but still cannot write to the DB. I have also check that there is full access to the HMI Any help would be greatly appreciated! Update 6/2/20: Adding the following software information that is being used to assist anyone that may have a solution: The original issue is that I/O fields are created and will not write to the PLC working memory or any DB. Values are entered into the fields during runtime, values are accepted and stay in the I/O field on the HMI, but never are written to the PLC.
------------------------------------------------------------------------------------------ |
Last edited by: J_Dole at: 05/29/2020 23:56:02Last edited by: Jen_Moderator at: 06/02/2020 08:15:29New subject after splitting Last edited by: J_Dole at: 06/02/2020 20:08:27Last edited by: J_Dole at: 06/02/2020 20:41:01 |
|
6/4/2020 12:27 PM | |
Joined: 8/3/2009 Last visit: 5/6/2024 Posts: 12884 Rating: (1645)
|
Hello check if the Tag you write in through the IO field is NOT used in a Recipe and if everything looks OK then try to reset the temporary files: https://support.industry.siemens.com/cs/de/en/view/109778709 Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on