5/24/2020 8:37 PM | |
Joined: 1/28/2012 Last visit: 11/22/2023 Posts: 21 Rating: (0) |
Hi, Experts. Need help to count the Product Per Minute to show on HMI as Line output or average/min, could you please help to make sample calculation program for S7 300 313 CPU , The maximum production rate is aprox 250 CPM. I tried with simple counting within time frame 1 min but it need wait 1 min to updating on time and not accurate. I am using Photo sensor to detect product at output conveyors, Unfortunately there is no HSC function in PLC ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/25/2020 11:36:49New subject after splitting |
|
5/26/2020 7:45 PM | |
Joined: 3/30/2020 Last visit: 9/20/2024 Posts: 4773 Rating: (981) |
https://support.industry.siemens.com/cs/ww/en/view/6170966 |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
5/30/2020 9:24 AM | |
Joined: 1/28/2012 Last visit: 11/22/2023 Posts: 21 Rating: (0) |
Hi , Thanks for your valuable feedback, as a maintenance guy I don't have much experience in PLC programming, However I have managed to build own a sample logic which is giving me good result: I used ADD in FC1 by incrementing +1 and this FC1 called in OB35 in cyclic interrupt set 20mS and in another FC2 I used counting logic and result transferred to DB ,, I would like to share if this can help someone or ignore it. AttachmentCount the Product Per Minute to show on HMI.pdf (410 Downloads) |
Follow us on