6/2/2020 10:00 AM | |
Posts: 36 Rating: (0) |
Hello everyone! I have a project with an 315-2DP: 6es7 315-2af03-0ab0 in Step 7 V5. Any suggestion what should I migrate to? Which CPU should I use instead of the "2af03". I made a test TIAP project to find out which modules can I use in TIAP too. The project uses some special FBs/FCs: I found the FB7 and FB8 in the TIAP library but how can I substitute the FC121 and FC122? What I have in the original projekt: What I put to my TIAP v13 projekt: I tried to migrate. But it doesn't work because some of the CPU and other modules are not available at V13. Any suggestion? Regards, Attachment01_Forum.zip (53 Downloads) |
Last edited by: hajleh12 at: 06/02/2020 10:03:02Last edited by: hajleh12 at: 06/02/2020 10:58:14 |
|
Follow us on