6/1/2020 12:59 PM | |
Joined: 9/21/2012 Last visit: 4/26/2024 Posts: 3923 Rating: (444) |
LGF library has a function that would be useful to your needs. |
This contribution was helpful to1 thankful Users |
6/3/2020 9:05 AM | |
Joined: 1/22/2018 Last visit: 4/10/2024 Posts: 31 Rating: (0) |
Thank you for your suggestion. I tried it, but it says that block is not supported by the CPU or global library version. I updated TIA portal 15.1 with update 4, and it remains the same. In this manual https://support.industry.siemens.com/cs/ww/en/view/109479728 it says: 1.2 Hardware and Software Requirements Hardware All blocks (FB, FC, DB,…) in the library can be used universally with the following controllers: • SIMATIC S7-1200 and SIMATIC S7-1200 F product family (from firmware V4.2) • SIMATIC S7-1500 and SIMATIC S7-1500 F product family (from firmware V2.0) • Simulation with SIMATIC S7-PLCSIM (from V14) So, it isnt compatible with ET200S PLC. Any other suggestions? THOMPSONvk |
Last edited by: Jen_Moderator at: 06/03/2020 12:30:34Optimized link. |
|
6/3/2020 1:33 PM | |
Joined: 1/22/2018 Last visit: 4/10/2024 Posts: 31 Rating: (0) |
I did it. Found this help: https://support.industry.siemens.com/cs/ww/en/view/43566349 Imported FC20 and TimeDB from this link, modified it to my project and easily get what i want. Thank you guys for your helping and suggestion. I m sending pdf with my network and function. It s work for now, i will simulate it couple of days to test it. BR THOMPSONvk Attachmenttimer_switch.pdf (35 Downloads) |
Last edited by: Jen_Moderator at: 06/04/2020 07:32:10Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on