6/2/2020 10:32 PM | |
Joined: 6/2/2020 Last visit: 8/23/2024 Posts: 215 Rating: (0) |
Is anyone know how to do tagging without using full address of TDC. |
6/3/2020 10:36 AM | |
Joined: 3/14/2008 Last visit: 9/24/2024 Posts: 2096 Rating: (938)
|
Hi, Can you specify your case? |
If I could help you, you can use the RATE button. Thank you. |
|
8/26/2020 3:26 AM | |
Joined: 6/2/2020 Last visit: 8/23/2024 Posts: 215 Rating: (0) |
Sir, As I have checked one C-script. It only contains setcolorstatus. So where I find all pre-defind colours?? |
8/26/2020 8:08 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi Harry55, you can find the code for the colors of the APL in the manual PCS 7 Advanced Process Library at section Central color management. With regrads |
8/26/2020 11:35 AM | |
Joined: 6/2/2020 Last visit: 8/23/2024 Posts: 215 Rating: (0) |
It wont help in my case. As I have checked in my TDC there is max int value is 64 and below 64 it changes 3 colors. So I want to know where is defined color with int value. |
Follow us on