6/3/2020 10:30 AM | |
Joined: 10/19/2016 Last visit: 9/16/2024 Posts: 309 Rating: (0) |
Hi sirs, I just made the automatic configuration for a 3 axis machine. I notice that Z axis has been assigned to the first drive (3:3:3), while it's physically linked to the 3:3:7 How can i change the topology? in general and channel DM i just set the 3 axis as (Z,TAV,SP1) and they are normally displayed on the main page. here the image (the attachment feature is not working correctly in Edge browser) |
𓋹 Siemens 840Dsl + TIA v17 𓋹 |
|
Follow us on