5/21/2020 10:09 AM | |
Joined: 11/24/2016 Last visit: 4/25/2024 Posts: 99 Rating: (4) |
Hi, I have a project on PCS7 V9.0 SP2 with Redundant CPU 410-5H. I have created a MultiProject that has 1 AS, 1 ES and and 1 OS Project with 2 Single Stations. I have configured my AS Hardware, ES Hardware and OS Hardware as per the manual. I have also created the Plant Hierarchy. One of the steps defined in the manual is to Assign an AS and OS to the Hierarchy Folder before CFC can be be placed. When I click the AS-OS Assignment for my Plant Hierarchy folder in AS, I can only assign the AS but there is no option available for Assigned OS. When I click the AS-OS Assignment for my Plant Hierarchy folder in ES, I can only assign the ES but there is no option available for Assigned AS. When I click the AS-OS Assignment for my Plant Hierarchy folder in OS, I can see the 2 Single Stations but there is no option available for Assigned AS. My question is that for is this how the AS-OS Assignment will be done. For the Plant Hierarchy Folder in AS only AS will be assigned but no OS, for Plant Hierarchy Folder in ES only ES will be assigned but no AS and for Plant Hierarchy Folder in OS which Single Station will be assigned? Thanks AttachmentAS-OS Assignment.zip (115 Downloads) |
Follow us on