5/21/2020 3:22 PM | |
Posts: 6 Rating: (0) |
s71200 + cm1241 (rs232)
I can get out of the thermal transfer printer from the computer via RS232C. When I connect plc instead of a computer, I can't print from the printer. Data must be sent as shown in exp1. When I send data through rs232 (cm1241) with PLC, it looks like exp2. therefore, the printer does not receive a print order. How do I send data like exp2 ------------------------------------------------------------------------------------------ |
Last edited by: haticedemirci at: 05/21/2020 15:23:36Last edited by: Jen_Moderator at: 05/22/2020 07:49:50New subject after splitting |
|
5/22/2020 9:52 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (817)
|
Hello,
eeeeehm probably you did mistake, you want better ask - How do I send data like exp1 not exp2 right? If yes, look to that exp1 lines of chars, there are simply lines not complete one sequence of chars. In this case probably after each line is some control byte/char also set, here I expect 16#0D (CR) so you need add to your PLC send buffer that bytes/chars after each sequence where line need to be cutted as in exp1. |
Last edited by: Duris_I at: 06/04/2020 19:27:25With best regards... |
|
Follow us on