6/2/2020 10:22 AM | |
Joined: 7/4/2018 Last visit: 4/18/2024 Posts: 16 Rating: (2) |
Hi, your situation is quiet the same as I but Im using 3 devices for my current project. 1. CPU 1511 2. IM 155-5 PN BA 3. IM 155-5 PN BA And I also use 2 router for communication. I connected my 1st router (configured as access point) to CPU using ethernet and from CPU I also connected my 1st IM. For my 2nd router (configured as client) I connect to my 2nd IM using ethernet. I already configured both router to able to communicate with each other but still, when I try to find accessible device, it only show my 2 device. Pinged all 3 devices using command prompt, all okay. [snip] Link above contains:- 1. Network view 2. Ping status 3. Accessible devices status Can someone help me with this? Seems like there's some setting i missed. ------------------------------------------------------------------------------------------ Attachmentcomm prob.zip (29 Downloads) |
Last edited by: Guru Strom at: 06/02/2020 10:33:49Last edited by: Jen_Moderator at: 06/02/2020 14:08:51New subject after splitting Last edited by: Jen_Moderator at: 06/02/2020 14:26:03Removed link and added all files as an zip file. |
|
Follow us on