6/4/2020 9:52 AM | |
Joined: 3/14/2008 Last visit: 9/25/2024 Posts: 2097 Rating: (938)
|
Hi, Please specify the PCS7 version (at least). It could be that functions may differ in the PCS7 versions. See attachment from the APL helpfile regarding errors in Local mode |
If I could help you, you can use the RATE button. Thank you. |
|
6/4/2020 10:14 AM | |
Joined: 3/14/2008 Last visit: 9/25/2024 Posts: 2097 Rating: (938)
|
Yes, You don't want a motor to start all of the sudden. Be aware that an operator at the HMI can also reset the motor. By pressing LocalStop, the motor will not start automatically after resetting. |
Last edited by: Oreca at: 06/04/2020 10:15:04If I could help you, you can use the RATE button. Thank you. |
|
Follow us on