6/3/2020 4:35 PM | |
Posts: 19 Rating: (0) |
I've added more screenshots and zipped them into one file.
AttachmentDebug.zip (65 Downloads) |
6/8/2020 1:03 PM | |
Posts: 19 Rating: (0) |
Hi Duris Ah, yes. Of course! Do you want to hear a funny story?....It now works! Don't ask me how. I've not changed anything. EDIT: Now that I remember correctly. The only thing I've done different is connecting the ethernet from the LMC600 (Channel 8) to P1 on the Scalance switch. I can't understand if this can result in anything different? I've added some more screenshots and zipped them. AttachmentProject_S7-1515_2_LMC600.zip (55 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on