6/9/2020 4:09 PM | |
Joined: 3/14/2008 Last visit: 9/20/2024 Posts: 2095 Rating: (936)
|
Hi MicroMan, Yes, this is possible, but you will need Plant Automation Accelerator which must be bought separately. The software is based on COMOS and is like (but much better) the previous AdvancedES software, where you could do bulk engineering by using Excel import list. You can create a configuration list in Excel. When you have created the CMT, the IO under the Technological Editor(green IO) can be edited in the PAA. You can map labels so PAA and PCS7 are connected. You can export the configuration to PCS7. See the PAA Overview page here Useful manuals for you: How do you import data into PAA with Excel import |
Last edited by: Oreca at: 06/09/2020 17:21:56Last edited by: Oreca at: 06/10/2020 07:07:04If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on