10/14/2019 12:51 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello IOT2000 Community, previously we published this applcation example to show you how to communicate over Modbus-TCP, OPC UA and S7 using Node-Red. This is the exact same example, but instead of using Node-Red we are using an Eclipse Project with a C++ implementation. The main benefit in using C++ is simply performance regarding execution and application start up time after boot. Feel free to give us feedback. If you happen to encounter compiler errors, please refer to this thread. Kind regards! AttachmentDoc_newc++.zip (693 Downloads) |
This contribution was helpful to10 thankful Users |
6/10/2020 12:27 AM | |
Posts: 47 Rating: (0) |
Thank you i was blind for sure. I got stuck on installing OPC UA and found that i can´t download .c and .h like seen on the PDF provided. So what do i do? |
6/10/2020 3:47 PM | |
Posts: 47 Rating: (0) |
Thank you, I see what you mean and solved the issue! |
This contribution was helpful to1 thankful Users |
Follow us on