5/14/2020 4:14 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665) |
Hello Rescobedo; I am not sure I quite understand your question. Do you mean, does the S7-300 CPU have a checkbox allowing PUT/GET accessibilituy? It does not. PUT and GET functions are accessible though communication FBs, as you can see in the following documents: Sample Program: S7 Communication with blocks FB14 ("GET") und FB15 ("PUT") of the CPU 317-2PN/DP https://support.industry.siemens.com/cs/ww/en/view/18924842 The sample project is complex, since it takes into account status and error bits of the functions. How do you program the function blocks FB14 "GET" and FB15 "PUT" in the S7 program of the S7-300 in order to transfer more than 160 bytes of data? https://support.industry.siemens.com/cs/ww/en/view/49450152 Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
5/14/2020 4:36 PM | |
Joined: 2/5/2013 Last visit: 4/23/2024 Posts: 320 Rating: (74) |
Hi Rescobedo, May be i am wrong for understanding your requirent but in case of S1200/1500 it is possible to put password to hardware side. If we put No access (complete protection) then it is not possible to access server PLC by client. I am searching manuals but we need to check whether it is possible for S7-300.May be there other options also. Br, AmolG. AttachmentPasswordProtection.pdf (190 Downloads) |
Please rate it. |
|
Follow us on