2/6/2012 11:38 AM | |
Posts: 10 Rating: (0) |
Hi there, Im making this program for a project. Its a washing machine program, but I need some help because I'm a little stuck.. Current program: Q1 is the pump(pumps water out) Q2 is water in Q3 is the thermostat Q4 is the washing engine. Now all the program does is pumping water out, letting water in, heating it, then the engine drives it around for x amount of time. tl;dr -I need help with getting the water out again, then get in new water to cleanse, then water out again, and then the engine takes it for a last spin to dry.
AttachmentVaskemaskin_2.zip (328 Downloads) |
2/6/2012 1:42 PM | |
Posts: 10 Rating: (0) |
Yes, I'm using a pressure switch (i3) i1 is start i2 is stop
|
2/6/2012 11:26 PM | |
Joined: 12/27/2006 Last visit: 4/15/2024 Posts: 1196 Rating: (113) |
I have a start for you. The trick is some reais RS row off. An RS relay switching your card in the previous step is completed. Then go to the next step Each step you make the functions with AND condition when an output to be. Converts for in this AND function is also at that the next step has not yet go through (be ready) has been. Each step you make the functions with AND condition to the next step. Need to exit more often than 1 time, then you make that out as an OR function and you have another condition to fix. If your laundry is clean, reset all relay RS. The program is certainly not ready, I have made the 2nd time intake water. here after you a while to rinse, then draining and then centrifugation. I must now go to bed .... Attachmentwashing.zip (389 Downloads) |
This contribution was helpful to2 thankful Users |
2/7/2012 2:26 PM | |
Posts: 10 Rating: (0) |
Oh wow, thanks :) Even though its a little too complicated for me.. there isnt a more simple way to do this, is there? Cheers
|
6/9/2020 8:51 PM | |
Posts: 5 Rating: (0) |
Here we are; asks me for username and password... |
Follow us on