6/15/2020 10:07 AM | |
Posts: 19 Rating: (0) |
Dear All I have an issue with 808d advanced. Setting the override key at 100%, set rpm (say) 700, output rpm at HMI and actual RPM do not match each other when spindle speed beyond 1000. It difficult to explain but I am trying. With 1: 1 gear ratio spindle rpm and HMI output at 100% override key must same value. I am getting it only bellow 1000 rpm. But when I PUT 5000 AT MD 32260 then actual rpm at drive become double but at HMI not. Any one have some suggestion for me?? Here is my spindle Motor specifications 1PH1103-1LD10-0GA0 Un=269, In=12.9 A, Pn=3.7 KW, Fn=36.9 Nn= 1000 rpm Imax=25.8, Max (NM)=70 Nmax=6000 RPM incremental 2500 ppr Drive Simanic V70 Spindle drive, Input= 3AC 380-480, 13.2 A 50/60 hz, Motor 3.7 Kw 1500 rpm 6SL3210-5DE21-1UA0
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/15/2020 13:32:03New subject after splitting |
|
6/15/2020 1:33 PM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 951 Rating: (13) |
Please don't post your question more than once -> closed. |
My Forum is the place to personalize your profile, |
|
Follow us on