6/17/2020 8:25 AM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
This trend diagram can a user not made in message text. It's only available in this LOGO! menü. |
6/17/2020 8:41 AM | |
Joined: 6/16/2020 Last visit: 11/14/2022 Posts: 9 Rating: (0) |
Thank you very much for answering |
This contribution was helpful to1 thankful Users |
6/18/2020 5:48 AM | |
Joined: 12/18/2014 Last visit: 4/23/2024 Posts: 32871 Rating: (4064)
|
If you have message texts active, press the cursor down until the start-up screen is displayed (if you have not changed it, it is the date & time display). Then press cursor right 3 times, then you will see the menu entry for the analog inputs 1-5. If the desired AI is not listed, then press the cursor right button again. Now you will see the menu entry for the analog inputs 6-8. Select the desired AI and press "OK". AttachmentLOGO! 8 manual 0BA8 2017_11 xxxx8-0BA0 page 88.pdf (465 Downloads) |
Follow us on