6/18/2020 2:40 PM | |
Posts: 47 Rating: (0) |
Greetings Siemens community, I am currently struggling with something very simple at first glance - the creation of a .emf file. I followed these steps: 1. Create a new pdl with dimensions e.g. 50x50 (width x height) 2. Create an object e.g circle 50x50 (width x height) 3. Insert a simple text field with the letter "M" in the middle of the ring 4. File -> Export as an .emf file In the attached .pdf file I have shown the result, picture 1 is what was saved as a .emf and picture 2 is what I got when I "called" the .emf with a "Graphics Object". As you can see, only the round shape and the color match the original :| What am I missing, I tried grouping all the objects before exporting - no effect. I tried creating a custom object same result. Thanks in advance. Attachment.emf creation.pdf (73 Downloads) |
Follow us on