1/9/2019 7:34 AM | |
Joined: 4/28/2015 Last visit: 3/15/2024 Posts: 3345 Rating: (372)
|
Hi, no. The IOT2000 itself runs the Linux OS. Of course you can use another PC with Windows to establish a SSH connection to the IOT2000 or to write programs for it. There are lots of examples about connecting the IOT2000 to a cloud. The engineering of the programs is mostly done on a PC running Windows, the execution on the IOT2000 running Linux. I hope things are bit more clear now Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on