6/11/2020 12:49 AM | |
Joined: 4/15/2019 Last visit: 3/4/2024 Posts: 27 Rating: (1) |
dear sir now you must make sure your ffs working in view open option and make sure you set read write edit for my pg it was and you can understand how to make it by opening C:\Siemens\Sinumerik\SinuComFFS if c: was where you setup and then open read me file warning wrong statment can kill data on card trust me it tried it before see fig-1 on attached aa file
if every thing ok you must see dos page like fig-8 after that you can see card contact like fig-4 we have to open sinumerik then nc arc dir you can found here your arc files on card for plc and nc copy them to any folder see fig-6 you must make sure you can see file extention ( windows control panel option file - un mark hide file extention ) you will have files like that _nc_arc rename it to NC.arc and make ok you can now open this file with sinocom-arc program see fig-9 to erise the card open cardware viewer in par you will found icon erise all data on card will removed card will show 0000000 0000000 in hex table :) open ffs again this time select open and open the working img abb file you clamed to have and select write dos windows will open erising card then transfare data to card then dos will closed after 100% after itsert the card you will have ncu 7-segmant run made 8-1-b-2-31-5 6 and stop on 6 after make plc nck rest about card you said you have of s7 400 - have a try but i am not sure you need to play with it if the old card readed and you have img good luck Attachmentaa.zip (91 Downloads) |
i m the toy maker so i love siemens |
|
This contribution was helpful to1 thankful Users |
6/19/2020 3:07 AM | |
Joined: 4/15/2019 Last visit: 3/4/2024 Posts: 27 Rating: (1) |
good try at all make sure you get the same software version on the card |
i m the toy maker so i love siemens |
|
Follow us on