6/29/2020 9:36 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi GabrielG, the APL-blocks use the attribute "S7_shortcut" to transfer the identifier to the OS. The default texts in ES are configured in the default library in English for the "s7_shortcut", "s7_unit", "S7_string_0" and "S7_string_1" attributes. Configure these texts in the language that is intended for the operator (plant operator) on the OS. For more Information about the configuration of texts and languages in SIMATIC PCS 7 see the application example Configuration of Texts and Languages in SIMATIC PCS 7. With regards |
This contribution was helpful to2 thankful Users |
Follow us on