6/18/2020 8:36 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, It could be numerous of things. It looks like something with enumerations from the look of the synchronization editor? I suggest you do synchronization step by step. One CMT at a time synchronizing with the plant project. Try to update the enumerations in all projects first. Which software are you running? If you have CFC V9.0 SP3 Upd5 installed, there is a restriction with CMT variants. If you have variants and the variant block has several output connections, interconnections could get lost. Upd5 is the latest update, but comes with this restriction. Maybe this could be an issue. Try to zoom in deeper in the synchronization editor, pointing to the variable that has the problem. Sometimes there is still strange behaviour… it will take trial and error to find the problem..
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on