6/28/2020 4:20 PM | |
Joined: 12/18/2014 Last visit: 4/19/2024 Posts: 32847 Rating: (4061)
|
Here is a suggestion. From Modbus you have to write the value into the VW2, if it is INT. If it is a DINT, then in the VW0.
Attachmentpero987_dimmer_control_0BA8.Standard.zip (230 Downloads) |
Last edited by: ixo65 at: 06/28/2020 17:33:09Attachment changed |
|
6/30/2020 7:00 PM | |
Posts: 6 Rating: (0) |
Thanks for yours suggestions. Was really helpful. After a few changes I'm happy how program works, but at the moment I don't have AM2 AQ (just ordered) so can't test. And I have question: 1. AQ output is from 0 ...1000 which is 0...10V, what if values to AQ are above that? in my case max 1500. output still will be 10V ? If I good understands everything above 1000 is still 10V ? 2. Is any chance to simplify my program? To save memory in LOGO Attachmentpero987_dimmer_control_V2.zip (217 Downloads) |
6/30/2020 8:10 PM | |
Posts: 6 Rating: (0) |
That's Ok thanks for the quick reply. |
Follow us on