6/30/2020 8:49 PM | |
Joined: 12/27/2018 Last visit: 9/18/2024 Posts: 510 Rating: (43) |
Friend You can update firmware in many ways. No need to Change anything on physical connection or PLC. Its very simple. There are 4 simple methods. Method 1. Same as reply from Qwazee. However no need to delete or change device,only update the firmware by Rt click on the device.Compile the program them download to PLC. Method 2. Update Firmware by Memory card; If you have TIA Portal V14 above, then you can download firmware to memory card, then just insert to PLC. Method 3.For lower version of TIA Portal(V12), download firmware from siemens website and, Go online to PLC by TIA Portal V12, go to diagnostic, then Browse Firmware in your laptop, then download. Method 4. If you don't have TIA Portal latest version, then Update Using a free Siemens software- Simatic Automation tool For your case, most simple method is just download firmware from Siemens website or latest Simatic automation tool have it that file and no need to download.Since you don't have latest license for TIA Portal, download free software Simatic Automation tool from Siemens website. Download firmware to PLC. Lower versions of Simatic automation tool are free from Licencing. Download Simatic Automation Tool No need to alter program or device.This is my Technicians mostly do at site location without TIA Portal. See the attached video for your reference and clear understanding. If you tell me which is your TIA Portal version, then I can explain you anyone most best method from above in more depth. Reference: One my old post contains details about Automation tool |
Last edited by: JKV JAMES ❤️(König James) at: 06/30/2020 20:51:35Last edited by: JKV JAMES ❤️(König James) at: 06/30/2020 20:58:59Last edited by: JKV JAMES ❤️(König James) at: 06/30/2020 21:23:52Jinson James, M.Tech (Power Electronics and Power System), |
|
Follow us on