6/29/2020 4:11 PM | |
Posts: 7 Rating: (0) |
Hi all, I have a server project in a computer and a client runtime in another PC (no project in client). The connection works. My problem is that, in the client PC, User Archive's table headings show the name of the fields, and not their alias. In addition, the client visualization symbology is wrong, it seems that it doesn't load the correct font (Windings?). The server project works and looks fine. I attach two snapshots to see the difference. How can I fix these two issues? Thanks in advance.
AttachmentClient-Server visualization.zip (44 Downloads) |
7/1/2020 1:34 PM | |
Posts: 7 Rating: (0) |
Hello bg2492, Changing the client Runtime language solved the table headings. How to add the Webdings font in the client project? Thanks! |
Follow us on