6/30/2020 4:36 PM | |
Joined: 5/12/2006 Last visit: 4/25/2024 Posts: 22227 Rating: (2980)
|
Hi, which buffer exactly you mean? Christoph |
This contribution was helpful to1 thankful Users |
7/1/2020 2:23 PM | |
Joined: 4/28/2015 Last visit: 9/20/2022 Posts: 1278 Rating: (295) |
Hi, I do not understand why the telegram lengths is confusing you. The telegram is used for the cyclic communication part. Reading the warning buffer is done acyclically without the telegram. But anyway: If you want to have your project similar as the application example you can simply switch your standard telegram 1 to 352 - all connections will be resolved automatically by the tool. Telegram 352 contains the same information as telegram 1 but some more feedback signals. There is also a very simple control FB for telegram 352 such as the SINA_SPEED FB for telegram 1. Here find the FB for telegram 352 which makes it easy: https://support.industry.siemens.com/cs/de/en/view/109747655 (see LSinaExt library) |
Best regards, |
|
This contribution was helpful to1 thankful Users |
Follow us on