9/24/2015 12:02 PM | |
Joined: 9/24/2015 Last visit: 8/2/2024 Posts: 19 Rating: (0) |
Hi, Why when I shut off and on the voltage in LOGO! 0BA8 the size/format of csv file change such as in attached in line 8 to 9, and result it's usless. Thanks Attachment192.168.0.2_2015-9-24 10-50-57.zip (246 Downloads) |
7/1/2020 9:44 PM | |
Joined: 2/5/2015 Last visit: 9/13/2024 Posts: 127 Rating: (0) |
Hello friends, I have the exact same problem asAle.Bon.ITA. Any suggestions to solve it? Any news about this issue? Regards. |
7/2/2020 5:10 AM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33792 Rating: (4197)
|
No. Start a Support Request. |
7/2/2020 4:52 PM | |
Joined: 2/5/2015 Last visit: 9/13/2024 Posts: 127 Rating: (0) |
Hi ixo65, My Logo! is 6ed1052-1fb00-0ba8 fs02. So it means it can´t be updated? I was taking a look at this other topic https://support.industry.siemens.com/tf//WW/en/posts/where-i-cat-get-new-firmware-for-logo-8-need-to-update/146432?page=0&pageSize=10 and it seems mine can´t be updated. Is that it? Thanks.
|
7/2/2020 4:56 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33792 Rating: (4197)
|
By LOGO!s with order numbers 6ED1 052-XXXXX-0BA8 and FS02 (Firmware V1.08.02) can't the firmware not updated. AttachmentVersions of 0BA8.txt (167 Downloads) |
Follow us on