5/11/2020 1:05 AM | |
Joined: 10/7/2005 Last visit: 9/22/2024 Posts: 3021 Rating: (1054) |
Hi Mayilsamy best I (well Siemens) can offer at this stage for DP Slave integration into an S7-1500 R/H systems is as per THIS FAQ (and I personally doubt this aspect will improve with future S7-1500 R/H versions) |
Cheers |
|
This contribution was helpful to1 thankful Users |
6/25/2020 3:12 AM | |
Joined: 10/7/2005 Last visit: 9/22/2024 Posts: 3021 Rating: (1054)
|
Hi Mayilsamy KM You can of course use a S7-1500 (with connected DP Slaves) instead of a S7-1200. If that is still not good enough for your customer, either a
|
Last edited by: fritz at: 06/25/2020 03:26:42Cheers |
|
7/2/2020 6:28 AM | |
Joined: 10/7/2005 Last visit: 9/22/2024 Posts: 3021 Rating: (1054)
|
Somewhat nice idea, but that is not possible. A PN/PN coupler allows for data exchange between two I/O Controllers (PLC's) and is NOT capable of having only I/O devices attached to one end of it. |
Cheers |
|
Follow us on