7/2/2020 4:23 AM | |
Joined: 3/3/2020 Last visit: 7/24/2024 Posts: 2 Rating: (0) |
GOOD EVENING EVERYONE. I HAVE TO REPLACE A SERVODRIVE WITH ANOTHER WITH A DIFFERENT ENCODER MODEL. I DID ALL THE PROCEDURES TO REPLACE IT WITH THE S7 TCONFIG. HOWEVER A FEW HOURS LATER, SERVO BEGAN TO PRESENT THE FAULT: "7900 ENGINE LOCKED / SPEED CONTROLLER IS LIMITED". WHAT SHOULD I DO TO SOLVE THIS PROBLEM? SOMEONE HELP ME PLEASE PS: I'm new to the field, I'm still learning, so bear with me ... :-D ------------------------------------------------------------------------------------------ |
Last edited by: MarcioNunes at: 07/02/2020 04:26:07Last edited by: MarcioNunes at: 07/02/2020 05:02:23Last edited by: Jen_Moderator at: 07/02/2020 05:55:49New subject after splitting Last edited by: Jen_Moderator at: 07/02/2020 05:56:15Edited text for better reading. |
|
7/2/2020 4:59 AM | |
Joined: 3/3/2020 Last visit: 7/24/2024 Posts: 2 Rating: (0) |
sorry, I didn't realize that the translator was on. |
7/2/2020 9:12 AM | |
Joined: 11/15/2015 Last visit: 9/3/2024 Posts: 179 Rating: (28) |
Dear MarcioNunes You are very welcome. have a look at fault No 7900: motor locked/ at high speed limit reached error 207900 Drive: Motor locked/speed controller at its limit (motor phase changing) Regards, |
Look for alternative not for the correct answer...if this is helping you rate it. |
|
Follow us on