5/2/2006 9:18 AM | |
Posts: 1084 Rating: (72)
|
Hi, You are right about that. It's very useful, but no wincc does not have it. with regards, Ikkezelf |
5/3/2006 9:45 AM | |
Joined: 1/17/2006 Last visit: 7/19/2024 Posts: 800 Rating: (63) |
Hi Stelns, I always use WinCC within PCS7. So I do not know if this will work. I can not try so please let me know if it will work for you? If you never used this. I will make you very happy. When you can work with this you can make pictures in no time.[:P] First you have to place the attached files into: C:\Program Files\Siemens\WINCC\wScripts\Wscripts.enu (or where you installed wincc). Then start the Dynamic wizard editor (hope you have installed it, its a WinCC tool) Start->SIMATIC->WinCC->tools->Dynamic wizard editor. Within this tool select Create DWD. Then startup your graphic designer and select the toolbar Dynamic Wizard within Toolbars. Whithin the tab pic. you can find 3 wizards Export picture objects and Import picture objects and change picture objects. Export Picture objects If you export objects just use a standard library picture of WinCC (created with the OS-editor). Then you can see what will happen. So open a picture with customized object in it and run the wizard. In the controll file you can select witch collums (and properties) must be exported and imported again. Import Picture objects It will speak for it self. Change picture objects When you change someting in a typical. Just play with it half a day and you can save a lot of time. I hope this will also work within WinCC (without PCS7). Good luck, Jaap Attachmentfiles.zip (514 Downloads) |
Follow us on