7/3/2020 12:26 AM | |
Posts: 1 Rating: (0) |
Hello A LOGO! Is 0BA8 compatible with LOGO Soft version 7.0? |
7/3/2020 5:17 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066)
|
No. For a LOGO!8.Standard you need at least LSC V8.0. But if you have a full version of LSC V7, then can you upgrade to the actually LSC V8.2.1 for free. You can download the upgrade from this web site: LOGO! Soft Comfort V8.2 SP1 (download, notes, instructions) After the download you must start the setup as an administrator. |
Follow us on