9/1/2020 10:15 PM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi , You can create a S7 connection between the CPU's of different versions. You can do this via TCP/IP or ISO for example. You can use different protocols like put/get to setup communication. Netpro should be configured for this. One thing to remember is that if you have clients or servers looking at servers from different projects which are gonna be different PCS7 versions, then this will not work anymore (Server packages). The PCS7 versions must be equally.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
9/1/2020 10:23 PM | |
Joined: 8/7/2015 Last visit: 2/15/2024 Posts: 11 Rating: (0) |
Thanks Oreca, I already made the link based on this link since both projects are in different multiprojects. but I have an error in the communication. https://support.industry.siemens.com/cs/ww/en/view/43033406 With what you mention of servers with a different version, you are right you can not see. I need communication to control between different projects. |
Last edited by: Jen_Moderator at: 09/02/2020 08:14:04Optimized link. |
|
9/2/2020 7:10 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi, Which error are you getting? And which type of PLC's are you communicating? Maybe you can post a print screen? |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on