6/11/2020 8:40 PM | |
Joined: 2/1/2019 Last visit: 4/16/2024 Posts: 21 Rating: (0) |
Dear All, I would like to connect a TA3115 Temperature transmitter to a Analog Input Card (6ES7 331-7NF00-0AB0). I do not know how to do that. I wanted to use 4-20mA signal with 1 wire, but it looks to me it is not possible. Here is a link about the sensor: https://www.ifm.com/il/en/product/TA3115 For some reason I could not upload a picture, despite the fact, that the size of it is just 800 kb. So I have 4 wire coming from the sensor. A white (as I know the current is coming on this), black, blue, and brown (+24V). Could you tell me how to do that? Which wire goes to where? Do I need to use a scaling function to scale after I wired the sensor? Best regards, |
6/11/2020 10:19 PM | |
Joined: 9/21/2012 Last visit: 4/25/2024 Posts: 3923 Rating: (444) |
Why don't you look at the Analog input manual, and the sensor manual, end see the connection examples? |
This contribution was helpful to2 thankful Users |
7/3/2020 4:40 PM | |
Joined: 2/1/2019 Last visit: 4/16/2024 Posts: 21 Rating: (0) |
It worked! :) Thank you. |
This contribution was helpful to1 thankful Users |
Follow us on