Industry Online Support
Technical Forum
7/3/2020 5:12 PM | |
Joined: 5/29/2009 Last visit: 11/24/2020 Posts: 10 Rating: (0) |
Do we need the PN driver software for this application case? In the webpage link, it mentioned a runtime license is needed. I am struggling with this topic. I only have the DLL file in the example code. based on the reference document, if I disable all the internet property items. I won't even find the S120 device using that x150 port. The LabVIEW code always stuck at the servo drive component 301 failure code. But the XML start error code is 0 which means the set up is correct. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/06/2020 08:07:46New subject after splitting |
|
Follow us on