8/11/2019 9:12 PM | |
Joined: 9/21/2012 Last visit: 4/25/2024 Posts: 3916 Rating: (444) |
Have you used TIA Software Updater? It automatically downloads HSP's for installed TIA softwares. |
7/7/2020 2:08 PM | |
Joined: 5/29/2014 Last visit: 4/16/2024 Posts: 56 Rating: (27) |
In the case of managed SCALANCE switches, You can usually download a GSDML file from the webserver of the switch itself if there is no up-to-date HSP in the hardware catalog. Some switches can only be implemented via their GSDML, as no HSP versions exist - I've had this happen. See https://support.industry.siemens.com/cs/document/89255256 The page states that "GSD is not a replacement for an integration in the hardware catalog", but when Siemens support themselves tell me that this is the only option available... In any case, I haven't had any problems using the GSDML in my project (I even set up a MRP ring topology), so I'm not sure what functionality might be missing from the GSDML. |
Follow us on