7/4/2020 10:22 PM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32871 Rating: (4064)
|
The LOGO! cannot do float values, only integers. Therefore it is rounded. |
7/6/2020 5:39 AM | |
Joined: 12/18/2014 Last visit: 4/24/2024 Posts: 32871 Rating: (4064)
|
Yes, with a combination of an analog comparator and the mathematical instruction and other blocks is it possible. |
7/9/2020 4:59 PM | |
Joined: 6/20/2020 Last visit: 4/4/2024 Posts: 42 Rating: (0) |
Oh ! sorry, i wrote in a translator but copy the french text... |
7/9/2020 6:10 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
A nice way to add flows for volume calculation or e.g. voltage and current for energy meter you can see in attachment. This is a tank filler for manual or automatic mode another person have asked for. The flow is added every second in an arithmetic block. If full liters are reached, an up counter will be increased and full liter is subtracted from the arithmetic block. To avoid overflow (value>32767), full liters are subtracted up to 8 times per 1-second-cylce. Use this program as you need or ask for details, Scorp AttachmentFlow1.zip (126 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on