7/10/2020 2:31 PM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
Do I need to have source code for PLC or can I change it on the control itself ? |
7/11/2020 6:31 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
No you cannot modify PLC on control in 802D. You need PLC tool 802D & PG/PC with RS232 port. HTH |
7/11/2020 9:10 PM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
But do I also need the source code or can I simply download the whole PLC program and change it ? |
7/12/2020 10:45 AM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
I only have the backup for the controller from manufacturer. Is that enough? And of course the controller itself. |
7/12/2020 10:56 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
NO |
7/12/2020 11:17 AM | |
Joined: 6/13/2019 Last visit: 9/14/2023 Posts: 139 Rating: (0) |
I have computer connected with rs232, i have 802D plc application and the controller. |
Follow us on