7/6/2020 12:39 PM | |
Joined: 11/15/2015 Last visit: 4/21/2024 Posts: 178 Rating: (28) |
Dear banci Yes this download only Japanese But, The new standard (Hermes) is TCP/IP- and XML-based and would replace the SMEMA standard that's been in effect for more than 20 years. Regards, |
Last edited by: ahmed2988 at: 07/06/2020 12:42:56Last edited by: ahmed2988 at: 07/06/2020 12:44:06Look for alternative not for the correct answer...if this is helping you rate it. |
|
This contribution was helpful to1 thankful Users |
7/6/2020 12:50 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello banchi; This link from Siemens Japan is the one you are addressing in your post? Or does it discuss similar issues on suface-mount technology communications for assembly lines? https://new.siemens.com/jp/en/products/automation/systems/industrial/plc/s7-1200/semi-a1.html “SEMI SMT-ELS (Surface Mount Technology - Equipment Link Standards)” is the Standards suite for SMT assembly line that replaces SMEMA interface and adds data communication capabilities to make assembly line smarter. Note: SEMI SMT-ELS application is only supported by Siemens Group in Japan. http://www1.semi.org/jp/SEMI_SMT-ELS Hope this helps, |
Last edited by: dchartier at: 07/06/2020 13:12:04Last edited by: dchartier at: 07/06/2020 13:16:30Last edited by: dchartier at: 07/06/2020 13:30:34 |
|
This contribution was helpful to1 thankful Users |
3/1/2021 11:16 AM | |
Posts: 1 Rating: (0) |
Hi banci, you can also use upgrade kits to have hermes within old smema legacy equipment. The main adavantage you can also solve the reinsert with this solution. Here you can check the details: SMEMA Hermes Bridge | Scheid IT | Deutschland (scheid-it.com) There is also a short movie, product flyer and the use cases. Regards, misterpostman |
Follow us on