7/7/2020 10:56 AM | |
Posts: 24 Rating: (0) |
Hi, There was a node developed for the usage of the access input pins, user button and multi-colour user LEDs for IOT2040. It can be found here: https://support.industry.siemens.com/tf/ww/en/posts/access-input-pins-user-button-and-multi-colour-user-led-from-node-red/161073?page=0&pageSize=10 My question is if it is also working for the IOT2050 hardware or if we have another package available. Besides, I would want to know with which Arduino it is compatible (with IOT2040 it was with Arduino 3). Thanks! Laura |
7/7/2020 11:41 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi, for the inputs, outputs and LEDs there are already pre-installed nodes in the IOT2050. For the User Button there is no node, but here you can find a workaround. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on