7/8/2020 5:22 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32879 Rating: (4064) |
Update 2 is available for SIMATIC Safety Matrix V6.3 Note Please refer to the readme file for further information on the enhancements and corrections. Before installation, read the product information in the Readme file. Under the existing article number for Safety Matrix V6.3, the current version Safety Matrix V6.3 Update 2 is automatically delivered upon availability of the update. |
This contribution was helpful to1 thankful Users |
Follow us on