7/7/2020 7:46 PM | |
Posts: 6 Rating: (0) |
Hi What can I do if my IOT2050 no longer boots from the eMMC? The boot order is set as follows: 1. eMMC 2. SD card. The status LED lights up red after a certain time after power on. How can I reset the Iot2050 to factory settings? Thank you very much for your help. ------------------------------------------------------------------------------------------ |
Last edited by: Wretch at: 07/07/2020 19:49:04Last edited by: Wretch at: 07/07/2020 19:51:22Last edited by: Jen_Moderator at: 07/08/2020 08:48:46New subject after splitting |
|
3/2/2021 3:20 PM | |
Posts: 6 Rating: (0) |
I have the same problem, I just unpacked the device, powered it on and the STAT LED turns from initially green to solid red after a few seconds. Edit: I've used the debug port to connect and check the bootloader output:
https://support.industry.siemens.com/tf/ww/en/posts/boot-problem/243833/?page=0&pageSize=10 Can you point me to what to do now or where to look how to fix this?
PS: The device will boot from an SD card when I flash the example image onto it. |
Last edited by: stockipa at: 03/02/2021 16:46:05Last edited by: stockipa at: 03/02/2021 16:49:17Last edited by: stockipa at: 03/03/2021 07:05:30 |
|
3/3/2021 12:40 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi, there is no operating system pre-installed on the eMMc. The Industrial OS is supposed to be, but this is not the case at the moment. So if you need the Industrial OS, please send a PM to me with your email address. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to1 thankful Users |
Follow us on