7/2/2020 10:59 AM | |
Joined: 3/3/2018 Last visit: 3/21/2023 Posts: 11 Rating: (1) |
Hello, I am using The Example Project Provided By Siemens Which consists at Communicating S7-1200 and S7-1500 to Mindsphere Using MCIOT extension without Having To add a gateway. I tested the Project on a S7-1516 and It worked Perfectly But WHen testing On s7-1214 FW V4.4.1 that did not Work and I am getting A message Error Like in the image Below. Is there any possible SOlution To this Problem? Project Link : https://support.industry.siemens.com/cs/ww/fr/view/109772284/en Thank You. |
Last edited by: Jen_Moderator at: 07/02/2020 13:46:52Optimized link. |
|
7/2/2020 2:06 PM | |
Joined: 3/3/2018 Last visit: 3/21/2023 Posts: 11 Rating: (1) |
Of course. I am using TIA Portal V16 Upd1 and I upgraded The PLC to FW4.4.1 |
7/9/2020 8:28 AM | |
Joined: 3/25/2009 Last visit: 9/21/2024 Posts: 1 Rating: (0) |
I got the same fault at S7-1215 DC/DC/DC V4.4.1. Hope someone can fix this bug soon. |
10/1/2020 9:38 AM | |
Joined: 4/7/2015 Last visit: 9/20/2024 Posts: 1 Rating: (0) |
Hi, I have the same problem with V16 and FW 4.4. And With V16 Upd 2 and FW 4.4.1 And With S7-1500 FW V 2.8.2 Attachment2020-10-01 09_38_21-Siemens - D__Dossiers_Pboulet_Bureau_MindConnect_109772284_LMindConn_MQTT_LMin.png (147 Downloads) |
Last edited by: mantelec@etn.fr at: 10/01/2020 16:23:35 |
|
Follow us on