7/10/2020 6:05 PM | |
Joined: 3/25/2008 Last visit: 4/3/2024 Posts: 240 Rating: (2) |
Thank you again to all, I create 2 server on the VMware and vorking but i have a new question: When i download the project on the server, all ok but the project is downloaded only in the selected server not in both server I need manually download in the second server. it seems that there is no redundancy, instead I checked the redundancy cards setting in WCC and with simatic shell, it seems all ok Anyone have a suggest ? thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/13/2020 06:49:31New subject after splitting |
|
7/10/2020 6:16 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, the first download must be a full download to both servers manually. After full download, changes can be done. So, yes you will have to do this manually |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on