7/10/2020 9:22 PM | |
Posts: 2 Rating: (0) |
Hi, has any of you used FBs from given examples? (https://support.industry.siemens.com/cs/ww/en/view/58638283 ) I noticed that my GPRS module goes to ERROR state because of area length error in FB100 - please find image attached. further investigation led us to line 113 in FB100: #smsParam.errors[#statPhoneNumber]:=#statStatus; If state changes from IDLE (where #statPhoneNumber is set to 0) to ERROR (where line 113 is called) area length error occurs because smsParam.errors is an array[1..10] - so there is no smsParam.errors[0]. Could anyone confirm this is a mistake in example code and should be corrected? Thanks in advance! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/13/2020 07:16:51New subject after splitting. Optimized link |
|
6/26/2021 5:31 PM | |
Joined: 12/31/2016 Last visit: 3/30/2024 Posts: 9 Rating: (0) |
lucijaaa, did you get a work around on this as i am having the exact same issue |
Follow us on